Building information modeling is rising to the top in the construction industry. But how does BIM contribute to a smarter, faster and greener industry? Let’s get the answers from Matteo Gianninoto, BIM Coordinator at Tecnoprogetti SA.
Matteo Gianninoto, BIM Coordinator at Tecnoprogetti SA.
Matteo Gianninoto started working as an MEP Designer very early on in his career. He explains that the specialisation was a real eye-opener that made him realise that it was time to explore new working methods:
“I read about BIM, experimented with some software and became captivated with its multifaceted potential. So, I decided to get a certificate and become a BIM Specialist”, says Matteo.
Soon after, he became a BIM coordinator tasked to implement BIM for AG&C associati. Although he still collaborates with the company, he’s currently employed as a BIM coordinator at Tecnoprogetti SA studio, where he works with internal training and design.
So, what value has BIM provided so far? And in which ways does BIMobject help to alleviate his work? Let’s dive into it.
BIM, short for Building Information Modeling, is a highly collaborative and intelligent 3D model-based process for managing information across a construction project’s lifecycle.
The methodology harbours data about a model’s physical and functional components, which gives architecture, engineering and construction professionals the insights and tools to plan, design and construct in a smarter, faster and more sustainable way.
The perks are plentiful for professionals and the world alike. For Matteo and his role as a BIM coordinator, he’s highly aware of them all. However, there’s one personal benefit that stands out a little extra:
“The methodology gives me greater control over the construction phase and site. Coordination is improved, which minimises cost and reduces the probability of errors.”
BIM isn’t a method meant for one, two, or three people. It’s a way for an entire project team to share information about a project – from concept to construction and maintenance. Matteo explains:
“BIM enables real-time collaboration between all stakeholders involved in a project, which leads to smoother communication and improved time efficiency.”
BIM plays a massive part in improving communication and resource efficiency in the construction industry. But that’s not all. The method offers a way to make (environmentally) conscious decisions on which components to include and to calculate precise material needs to reduce waste. Matteo explains:
“Sustainability is a subject that must be approached with utmost importance and sensitivity. We must take it into account when we develop projects and select information components”, says Matteo Gianninoto.
The construction industry has flown under the media radar when it comes to our impact on the environment. The sad fact is that CO2 emissions from the building sector are at an all-time high, representing 38% of the world’s total. So, how can BIM contribute to a more sustainable world? Matteo explains:
“BIM gives architecture, engineering and construction professionals a holistic digital source of information. This is a great step forward when it comes to mitigating a project’s environmental impact.”
There’s no doubt that Matteo Gianninoto is a devout BIM enthusiast. But in a time without trade shows and accelerated digitalisation, professionals need a smooth way to pick the right BIM objects for their BIM projects. That’s where BIMobject enters the main stage.
“The BIMobject marketplace helps me in the design phase when products aren’t well defined through technical sheets. Although we have set dimensions for our machines and plant components, BIMobject helps to reduce the modelling time”, says Matteo Gianninoto.
BIMobject offers a digital marketplace where manufacturers can connect with architecture, engineering, construction and operation (AECO) professionals. The platform gives manufacturers a 24/7 365 way to reach architects and gives users – such as Matteo – free access to BIM objects as well as a direct line of communication with manufacturers.
But in which ways have the digital marketplace proven beneficial for Matteo’s daily work?
“BIMobject offers the possibility to choose between several BIM object families and the opportunity to use those which are relevant to the real characteristics with a satisfactory level of information. This makes the work smoother and lays out a foundation for better project development”, concludes Matteo Gianninoto.